2/18/2024 4:36 PM | |
Joined: 2/23/2017 Last visit: 2/18/2024 Posts: 37 Rating: (0) |
Hi, I made a simple "blinker" kind of program where the blinking speed is adjustable via the LOGO!'s keys. For any reason, the keys are not read instantly but mostly with a delay (can go up to two seconds). Why is this? What can I do to have the keys read much faster? AttachmentVitesse de clignotement réglable avec touches LOGO.zip (200 Downloads) |
2/18/2024 4:50 PM | |
Joined: 12/18/2014 Last visit: 6/4/2024 Posts: 33149 Rating: (4095)
|
You have no chance to make the cursor keys faster. The speed is integrated in the firmware. |
Follow us on