6/6/2015 6:32 AM | |
Posts: 93 Rating: (0) |
Hi all, i have CPU 412-2DP (6ES7 412-2XG04-0AB0) used in press operation. press operation auto mode suddenly cpu all LED blinking continuosly.and not able to going monitoring mode.what are the reason for this issue? how to identify which type of fault occur.pls guide me to solve this issue. For better understanding i attached the photo and video file while fault occured conditon.pls go through and any one reply me, fault occur more than 3times per day. now i off/on whole power and reset the fault in the last one week. pls support me. Advance thanks and Regards, Suryamuni Attachmentcpu stop mode.pptx (393 Downloads) |
Last edited by: Suryamuni at: 6/6/2015 6:49:55 AM |
|
6/6/2015 8:38 AM | |
Joined: 3/28/2015 Last visit: 5/15/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the attached file might help. Kindly post the diagnostic buffer for the CPU 412-2 AttachmentAutomation System S7-400 CPU.pdf (555 Downloads) |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
6/6/2015 8:43 AM | |
Posts: 93 Rating: (0) |
Hi all, Here i attached the video under fault condition for better understanding.pls anyone reply me. Regards, Suryamuni Attachment2.avi (394 Downloads) |
This contribution was helpful to1 thankful Users |
6/6/2015 9:24 AM | |
Posts: 93 Rating: (0) |
Hi, Thanks for your reply. here attached the diag. buffer,pls go through it. Regards, Suryamuni AttachmentDiagnose.txt (333 Downloads) |
6/6/2015 9:30 AM | |
Joined: 11/29/2011 Last visit: 5/7/2024 Posts: 1358 Rating: (231) |
Hi, When all LEDs start cycling it means the CPU went into an unresponsive state. The cause can be a many things from HW error to corrupted memory content or even EMC/power supply issues. Have a look at this thread:
Anyways if you check the CPU installation then maybe worth considering the CPU firmware upgrade as well. See this thread about these advices S7-400H Fault . I hope I could help! |
Last edited by: MicroMan at: 6/6/2015 9:32:20 AMLast edited by: MicroMan at: 6/6/2015 11:38:44 AMLast edited by: MicroMan at: 6/6/2015 8:45:43 PM- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
6/9/2015 2:48 PM | |
Joined: 1/28/2009 Last visit: 5/19/2024 Posts: 6840 Rating: (1359)
|
Hello, For updating the firmware of CPU for "6ES7412-2XG04-0AB0" V5.0 onwards, it is possible to update firmware in online mode.For your case,V4.1,You need "Flash 4 MB (article no. 6ES7952-1KM00-0AA0) or larger" to update firmware.Read more here: Firmware-Update for CPU412-1 and CPU412-2 I hope this helps, hdhosseini |
Follow us on