1/16/2024 12:17 PM | |
Joined: 1/12/2023 Last visit: 3/12/2024 Posts: 19 Rating: (0) |
Dears, I have installed on a IPC, PDT ETH v1.5 and when I try to connect a Panel IFP 15 will crash Windows in Blue screen of death (BSOD). If I install PDT v1.6 (without ETH) and I connected via DisplayPort + USB, there is no problem. I download software's from: https://support.industry.siemens.com/cs/mz/en/view/109792891 In menu IFP ETH, I set as documentations the IP's static for Panel. If I put Panel in LAN with PLC, then the Panel will appear and disappear in the list of IFP ETH, but if I put Panel in a LAN separately, just directly with IPC then is always appear in list because the panel have IP generated at 192.168.1.200. If I check "Connect automatically" then the IPC will crash many times. Sometimes if I open Chrome Browser and explore on it, the IPC crash. Can be an incompatibility with Chrome Browser? Sometimes at startup the resolution is automatically set to 5000x3000, but the maximum of Display is 1920x1080. Can be problems with Intel video drivers? Do you encountered the same problem? |
Last edited by: Jen_Moderator at: 05/08/2024 06:42:49Link optimized. |
|
Follow us on