4/4/2024 11:49 PM | |
Joined: 12/18/2023 Last visit: 4/4/2024 Posts: 3 Rating: (0) |
Hello every one i'm using simatic manager 5.5 + sp4 i've tried to install HW updates to add 6ES7155-6BU01-0CN0_V421 IM 155-6 DP HF in the catalog but do this through internet connection had failed so i downloaded hardware support packages from this link https://support.industry.siemens.com/cs/eg/en/view/23183356 but the problem that the file i've found was for old version 6ES7155-6BU00-0CN0_V1.1 IM 155-6 DP HF and the module i have is 6ES7155-6BU01-0CN0_V421 IM 155-6 DP HF so i need a way to update the firmware of the installed file or a new updated file to install i attached some photos of what i've that may help thanks in advance Attachmentim155-6dphf.zip (12 Downloads) |
Last edited by: ahmed215219 at: 04/04/2024 23:52:03Last edited by: Jen_Moderator at: 04/05/2024 08:56:41Link optimized. |
|
4/5/2024 5:37 AM | |
Joined: 3/11/2019 Last visit: 5/23/2024 Posts: 1433 Rating: (261) |
Hi, the new IM 6ES7155-6BU01-0CN0 is spare part compatible, means you can use the new one in real hardware but use the old product number in hw-config. It works fine. If there are any errors on the module, this has a different reason! Therefor, have a look in the diagnostics buffer. The IM 6ES7155-6BU01-0CN0 is sold in bulde 6ES7155-6BA01-0CN0. Hardware conversion for ET 200SP interface modules IM155-6PN/2 HF (PROFINET) and IM155-6DP HF (PROFIBUS)... are fully compatible with the predecessor modules and can replace them without the need for reconfiguration As an alternative, you can use the GSD file (not HSP) in V5.4. PROFIBUS GSD files: ET 200SPregards sancruz |
Feedback appreciated, please rate |
|
Follow us on