3/11/2024 9:07 AM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello Pankaj, Please have a look at the following link: How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
3/15/2024 1:52 AM | |
Joined: 3/13/2019 Last visit: 6/2/2024 Posts: 152 Rating: (2) |
Dear sir, Pls help on this Regards, Pankaj Tiwari |
3/20/2024 10:55 AM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1658)
|
Hello pankaj_054 Check all the steps in the basic example: https://support.industry.siemens.com/cs/ww/en/view/23802404 you should not use the "Auto" setting in PGPC Interface, use always the needed protocol. You can also check in the PGPC initerface settings at "diagnose" or your CP-> Profibus and read out the bus. then you should see your PC and the HMI as active partner on the bus Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on