4/26/2024 10:11 AM | |
Joined: 4/26/2024 Last visit: 5/2/2024 Posts: 2 Rating: (0) |
Dear colleagues, There is a redundant system on two physical IPC647D PN machines. The system is configured and working correctly. After changing the picture in TIA Portal15.1 and trying to upload to the server, the error "Check whether the SCS network adapter of the redundant operator station is configured and enabled" appears. Read and checked all settings according to the instructions and did not help "Redundancy in WinCC V7.x and WinCC Professional" (https://support.industry.siemens.com/cs/kz/en/view/109772627) |
Last edited by: Jen_Moderator at: 04/29/2024 06:31:26Link optimized. |
|
5/8/2024 1:38 PM | |
Joined: 8/3/2009 Last visit: 5/14/2024 Posts: 12944 Rating: (1647)
|
Hello Damir_EFC Check the basics. Often if the stations do not see each other in Simatic Shell something like imhosts files or similar is not set up correctly: https://support.industry.siemens.com/cs/de/en/view/108464289 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on