12/7/2023 9:46 AM | |
Joined: 11/18/2023 Last visit: 12/15/2023 Posts: 3 Rating: (0) |
I try to connect my laptop to NCU 720.2 of sinumerik 840Di sl via X127 port. CP config of project is 192.168.214.1. i set my laptop IP is automatic. Then i ping to adress 192.168.214.1, everything is ok.I can see IP adress, MAC adress of NCU, TCU, MCP..v..v in my system when use " Edit Ethernet Node" in Simatic manager. But i couldnt go online NCU, no download, no upload( Couldnt " Upload station to my PC"). My laptop use windown 7 64 bit. So, my question is: with windown 7 64bit, how can i online NCU 720.2 via x127. is there firewall in sinumerik 840Di sl which hamper the connection???? Plz help me! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/07/2023 12:47:04New subject after splitting and Text formatting optimized |
|
Follow us on