7/30/2023 8:32 AM | |
Joined: 7/15/2023 Last visit: 1/16/2024 Posts: 26 Rating: (0) |
Hi, I want to display weekly timer settings in the web gui. If I put 1 timer (cam) in LWE it works fine, fast and can see the changes on the logo display parameter settings. When I copy timer 1 on the web and change the block numbers etc. then the in/off switches for the weekdays are not working anymore for both klocks 1 and 2. The on/off times seem to work though. Attached the project. PS: I don't understand the concept of TagTable in LWE. Isn't that redundant with the parameter VW mapping in LSC ? Attachmentweeklyinweb.zip (269 Downloads) |
Last edited by: Domoticom at: 07/30/2023 08:35:22 |
|
7/30/2023 9:32 AM | |
Joined: 12/18/2014 Last visit: 6/7/2024 Posts: 33164 Rating: (4097)
|
I checked it with my LOGO! 8.3. I had no problems with with cam 1 and cam 2. |
Follow us on