4/22/2024 8:56 AM | |
Joined: 1/17/2020 Last visit: 4/25/2024 Posts: 3 Rating: (0) |
Hi, I have the same problem. I'm using Step 7 v5.6 SP2 - in hw list there is no 6ES7 315-2AG10-0AB0 v2.6 firmware, it's only v2.0. I tried to install HW Updates, downloaded it from Siemes website, but when I click on the 0125 CPU 315-2 DPV2.6 there is a message 'Selection not possible. Cannot install over a HW update supplied with the STEP7 version. Can You help me guys? Regards, PZ ------------------------------------------------------------------------------------------ |
Last edited by: p.zurek at: 04/22/2024 08:57:44Last edited by: p.zurek at: 04/22/2024 10:14:04Last edited by: The Helping Hand at: 04/22/2024 12:59:13New subject after splitting |
|
4/22/2024 2:16 PM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32982 Rating: (4076) |
I have installed all possible HW-Updates for STEP 7 V5.6 SP2. |
Last edited by: ixo65 at: 04/22/2024 14:19:34 |
|
4/23/2024 5:25 AM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32982 Rating: (4076) |
Start a Support Request. |
4/23/2024 5:47 AM | |
Joined: 3/11/2019 Last visit: 5/7/2024 Posts: 1399 Rating: (248) |
Did you also install the latest hotfix for V5.6+SP2? Download Hotfix 10 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2regards sancruz |
Feedback appreciated, please rate |
|
Follow us on