2/9/2024 1:09 AM | |
Joined: 4/3/2023 Last visit: 5/31/2024 Posts: 9 Rating: (0) |
Hi all, I am working with PCS 7 V8.2 and am running into an issue with one of my units when trying to use SIMATIC Batch. When I compile the batch, I get the warning "The block [block name] was not transferred to any OS". I am not able to access this unit or its phases in Batch. I display the associated unit block in WinCC, and that shows errors as well. I have tried to do a full compile of the OS, along with a Generate -> Propagate -> Merge and download of the batch with no luck. Does anyone have any idea what could be wrong here? Please see attached screenshots for exact warning messages. Thank you! AttachmentScreenshots.zip (105 Downloads) |
2/9/2024 5:20 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928)
|
Hi, The AS is compiled? If so, it could be that the folder where the unit is located does not have an AS assignment. You should check the plant hierarchy folder for correct AS assignment. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on