4/21/2023 10:33 AM | |
Joined: 1/31/2020 Last visit: 2/21/2024 Posts: 2 Rating: (1) |
Since there arent too much other discussions about this topic in existence: I'm using a STARTECH "DK30CH2DPPDU" USB-C Dock with the PG M6 Adv. Altough it isn't charging the PG's battery over USB-C & only 2 of its 3 aviable 4K Monitor outputs are being recognised, everything else is working as expected, so for my use case it's kind of the best solution I've been able to find. Still, the fact that every other Laptop / Windows Tab / Android Phone I ever used with that Dock did support all of its features, while running on much weaker hardware than my PG M6 adv. (i7 8850H, 1TB NVME, 2TB SSD, 64GB DDR4 ...), plus those mysterious BATTERY, WIFI and BOOTUP problems it started having half a year ago is making sure that I will never consider buying a FIELD PG again. Kind of sad, since I really enjoyed working with my PG M4 (that is still running flawlessly ) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/21/2023 10:56:17New subject after splitting |
|
Follow us on