12/29/2023 6:39 AM | |
Joined: 2/15/2019 Last visit: 6/4/2024 Posts: 2 Rating: (0) |
"Hello everyone, I need help with the ET200SP AI card 4-wire connection. In the attached picture, you can see all four wires coming from the AI module, but I want to provide external 24V to the transmitter. In the second picture attached, I have connected the external 24V. Is this wiring correct, or do I need to make adjustments? Your assistance is appreciated. Thank you." MLFB no AI Card 6ES7134-6GF00-0AA1 AttachmentET200SP_AI_Wiring.zip (181 Downloads) |
12/29/2023 10:49 AM | |
Joined: 6/19/2017 Last visit: 6/5/2024 Posts: 8139 Rating: (165) |
Closed cause question posted twice. The second thread with the subject ET200SP AI Card 4 wire connection is published within the conference Decentral Peripherie. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on