5/7/2024 6:14 PM | |
Joined: 4/25/2024 Last visit: 5/10/2024 Posts: 2 Rating: (0) |
This is an ancient thread. How can I get up-to-date information on commissioning a G120X drive into the TIA Portal? I downloaded the GSDML file from The SINAMICS G120X PROFINET GSDML files and PROFIBUS GSD files - ID: 109763250 - Industry Support Siemens In TIA Portal I do "Options/Manage GSD files" and browse to where the file was downloaded and extracted. I get "No items match your search". But Windows explorer shows "GSDML-V2.34-Siemens-Sinamics_G120X-20190426.xml" is present. So how do I load the GSDML file into TIA Portal V17? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/08/2024 06:56:27New subject after splitting. Link optimized. |
|
5/8/2024 9:18 AM | |
Joined: 4/5/2017 Last visit: 5/13/2024 Posts: 51 Rating: (7) |
Hi tjrob2, You need to select the complete unzipped folder to insert the GSD-Files to TIA. See: Kindly - Sina |
5/10/2024 8:24 PM | |
Joined: 4/25/2024 Last visit: 5/10/2024 Posts: 2 Rating: (0) |
Yes. I discovered that. It's unfortunate that the program has such a non-standard user interface. Thanks. |
Follow us on