6/22/2022 6:20 PM | |
Joined: 12/25/2016 Last visit: 6/1/2024 Posts: 90 Rating: (0) |
Hi. Is there any body who can send me link for the software in programming this CPU? thanks. |
6/22/2022 6:37 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095) |
You can program it with STEP 7 or with TIA-Portal when the CPU is not to old. |
6/22/2022 6:45 PM | |
Joined: 9/27/2006 Last visit: 6/5/2024 Posts: 12260 Rating: (2670)
|
Hello hyo_eddie; To program a s7-315-2DP, you have the choice of 2 different softwares: - Step 7 v5.7, the original programming for S7-300 and s7-400 CPUs; - Step 7 v17, the new TIA Portal software that allows you to program S7-1200 (in the Basic version) or S7-1500, S7-300 and S7-400 PLCs (in the Professional version). Siemens allows you to download either of these softwares in a trial format, which gives you unrestricted functionnality for 21 days, after which you will need to purchase and install a valid license from your nearest Siemens rep. These softwares are not compatible: you cannt open a Step 7 v17 program in Step 7 v5.7 or example. - STEP 7 V5.7 / S7-GRAPH V5.7 / S7-SCL V5.7 / S7-PDIAG V5.7 / STEP 7 Professional 2021 Trial Download - SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V17 TRIAL Download https://support.industry.siemens.com/cs/ww/en/view/109784440 Have you thought about a programming cable? If ou have a CP 343-1 (Ethernet communication provcessor) on the CPU rack you can use Profinet to download to the PLC. If you don,t you will need a MPI/Profibus adapter, the latest USB-PC A2 adaplter would be a recommended selection (6GK1571-0BA00-0AA0). https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/10204161 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on