5/19/2011 10:08 AM | |
Posts: 123 Rating: (4) |
Hi, we have servers running as master and slave(redondant) WinCC 6.2 is running on them. sometimes the master server is crashing, i have noticed on the WinCC_Sys_04.log file that the last line isa script problem when a crash append: "SCRIPT,ActionOverflow:more than 10000 Actions to work" is anyone faced the same problem ! thanks in advance for your help. log files of master and slave in attachment Sylvain
Attachmentlog files.zip (184 Downloads) |
5/19/2011 10:28 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
maybe this can help you: What can be the cause of the WinCC error message "More than 10000 actions in work" (up to V6.2: "More than 5000 actions in work")? https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=2357302&caller=view |
Last edited by: SteBo at: 5/19/2011 10:36 AMyou can also try to monitor your scripting before this error message comes up with APDiag: "C:\Program Files\Siemens\WinCC\uTools\apdiag.exe" or use the "GSC Diagnostics window" in your picture in Runtime. APDiag could find more errors than GSC Diagnostics window while switching pictures. Both can help in finding failing scripts and the reason why ... B r g d s , |
|
This contribution was helpful to1 thankful Users |
5/19/2011 10:28 AM | |
Posts: 799 Rating: (42)
|
Dear syl20, in the diagnostic file I saw, that there is script.log file. This file only exists, when there was a crash of the script. exe. Normally there is a little more Information in the logfile, but it seems to me, that the crash on your system is a very hard crash, so WinCC can't finisch the diagnostic entry in the logfile. You should check all your script with diagnostic traces or printf's and Global Script Windows or ApDiag. If error occurs furthermore, you should install the Dump tool from Microsoft. (Download here - how to use here). Then you have to configure the tool for an automatic dump of the script.exe process. This dump you have to send to technical support, with all other informations (exact WinCC Version/ when occurs the crash/ which cycle/ and so on) Hope this helps :-) best regards |
This contribution was helpful to1 thankful Users |
5/19/2011 10:43 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi syl20, I worked with WinCC V6.2 in several projects ago during installing sometime there are some files not installed properly. Some of the errors also have been fixed in the latest versions of the Hotfix: http://support.automation.siemens.com/WW/news/en/48168705 Try to install this Hotfix, it may help you. |
Last edited by: Khaled_Ezzat at: 5/19/2011 10:45 AMBest Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on