6/19/2023 7:52 PM | |
Joined: 6/19/2023 Last visit: 6/20/2023 Posts: 2 Rating: (0) |
Hi, I need help with programing, the logo 12/24RC. I am out of programming for almost 7 years. I need a simple program, where with one push button to start the action I need to start the same time one relay ( relay triggers the stepper motor or DC motor) and one pneumatic valve (releases a grease feeder), the valve needs to be open for approximately 0,5s ( I want to change time ), the same time I want the relay its come on as well, but need to be cut off on X time somewhere 3 to 5s. Also, I will need one actuator to operate as turning on when the valve goes out and turning off after x time (the time it's determined by dispensing value of the grease I need to apply on a gear. ( this actuator will be used as a vacuum for grease suction back from application nozles. Thanks in advance for your help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/20/2023 05:04:40New subject after splitting |
|
6/20/2023 12:38 AM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33166 Rating: (4098)
|
Something like this? |
Follow us on