Industry Online Support
Technical Forum
6/22/2023 1:56 AM | |
Joined: 10/15/2022 Last visit: 6/7/2024 Posts: 66 Rating: (2) |
Hi everybody. I made a demo program that generates a datalog. It makes a record in the datalog periodically and when an event occurs. An event is, for example, a change in the state of input I1 and/or output Q1. An analog input AI1 value is sent when it changes by more than 50 units. Logging is turned off by default. The logging interval can be changed from the second screen and logging can be turned on from the third screen (ESC >2s, OK, etc.). There are a total of three screen displays. Updated: Attachment contains program and his description. Program version is v.3. Tested on LOGO!8 6ED1052-1MD08-0BA1. Andrus ----- Translation: Google Translate
AttachmentData logging demo.zip (433 Downloads) |
Last edited by: Andrus_Saar at: 06/24/2023 10:32:33Last edited by: Andrus_Saar at: 08/08/2023 16:50:31 |
|
Follow us on