3/31/2024 6:41 PM | |
Joined: 3/10/2013 Last visit: 4/8/2024 Posts: 11 Rating: (0) |
Hi, I would like to know the best way to keep a bool parameter in high state in case of a power failure or simply when you turn the controller off and then turn it back on. I will connect a Logo! to an HMI, then I am going to set a flag from the HMI either on or off according to the requirements. I’m afraid that if I set the flag on and the power fails (which happens quite frequently) then when the power comes back on the flag will lose its on state. I came up with the attached circuit, will it work? Can you point me to a good solution if it has been discussed before? Thank you P.S. Please, excuse me if this a basic question, I’m still new to Logo! AttachmentRETENTIVE_BOOL_PARAMETER.zip (24 Downloads) |
3/31/2024 6:50 PM | |
Joined: 12/18/2014 Last visit: 6/13/2024 Posts: 33189 Rating: (4102)
|
I can't see anything except a network project with 2 LOGOs and an HMI. There is no program in either LOGO. |
3/31/2024 6:55 PM | |
Joined: 3/10/2013 Last visit: 4/8/2024 Posts: 11 Rating: (0) |
Please, excuse me. It is there, just scroll down and right. I am going to upload it again in a better position |
3/31/2024 7:02 PM | |
Joined: 3/10/2013 Last visit: 4/8/2024 Posts: 11 Rating: (0) |
Re-uploaded Now it can be seen without scrolling AttachmentRETENTIVE_BOOL_PARAMETER.zip (19 Downloads) |
3/31/2024 8:43 PM | |
Joined: 6/20/2010 Last visit: 6/9/2024 Posts: 89 Rating: (0) |
Hi , I didn`t understand what do you need, can you explain better? |
3/31/2024 9:22 PM | |
Joined: 6/20/2010 Last visit: 6/9/2024 Posts: 89 Rating: (0) |
Something like this example? do you know the retentive funtion in bloks? |
Follow us on