11/2/2022 11:39 AM | |
Joined: 10/5/2022 Last visit: 11/18/2022 Posts: 4 Rating: (0) |
Is LWE V1.1.1 available as a standalone download? I can only see it as a LSC V8.3 SP1 bundle. Thanks |
11/2/2022 12:28 PM | |
Joined: 12/18/2014 Last visit: 5/16/2024 Posts: 33043 Rating: (4082)
|
I don't think that it is a firmware issue. Firmware update V1.83.02 for LOGO! 8.3 basic devicesMy opinion is the installation of LWE is not correct because the transfer window doesn't show a interface. You can start a Support Request to ask Siemens directly. |
4/26/2024 1:01 PM | |
Joined: 4/26/2024 Last visit: 4/26/2024 Posts: 1 Rating: (0) |
Did you solve the problem?I have the same problem and have tried everything.Thank you |
Follow us on