3/8/2024 1:43 PM | |
Joined: 9/18/2023 Last visit: 6/7/2024 Posts: 2 Rating: (0) |
Hello, I'm trying to figure out how to make my 1510SP- 1PN and G120 CU240 E-2 PN communicate together. At the moment i can go online on both but i get a few error about communication on the plc, i'll put everything in the attachment. I tried a lot of things but i still cannot make it work. Thank a lot already for the help. AttachmentScreen.zip (111 Downloads) |
3/12/2024 1:49 PM | |
Joined: 9/18/2023 Last visit: 6/7/2024 Posts: 2 Rating: (0) |
Thank you for your quick answer, the unmanaged switch was in fact causing trouble, i now seem to have a communication with the G120. I have a second problem now, i actually removed the connection to a V90 to test only the G120 and made this post. I now need to add it to the network. Unfortunetly it's not working at the time, the V90 has a PN name and IP, and is set to IRT mode, the telegram i'm using are in the attachement, the whole topology is in green but the 2 LED are lit up ( Ready : Red and Com : Green). Do you have any idea what should i look for ? AttachmentScreen_2.zip (19 Downloads) |
3/12/2024 4:46 PM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22256 Rating: (2987) |
go onlien an check if a fault is present on the v90 |
Follow us on