4/26/2024 10:13 PM | |
Joined: 4/28/2015 Last visit: 5/13/2024 Posts: 6 Rating: (0) |
The focus on IOField only works if the screen is also "focused". When we open the same screen as a popup, the TIA don't put focus on this new popup screen and then the IOField don't get focus too. Only when the user click on the new popup already openned the IOField with TabIndex = "1" get the focus automatically. I've realized that the focus remains in the button when the user click on it in order to open the popup. Is there a way to set the focus to the popup? Or a way to set a "Onload" script to put the focus on some IOField placed on this popup? (sorry for double post. The Google Chrome fails to post my first attempt) ------------------------------------------------------------------------------------------ |
Last edited by: Gumulatinho at: 04/26/2024 22:16:59Last edited by: Jen_Moderator at: 04/29/2024 08:45:31New subject after splitting |
|
Follow us on