11/25/2009 1:56 PM | |
Posts: 510 Rating: (117)
|
I did not find SoftShop in the CA01 Catalog so Siemens no longer sells it. Fastrak Softworks was the original developers of Softshop and they still sell a 505 programming package. The link is http://www.fast-soft.com/and the package is PLC Workshop. There is also a MSDOS based programming package, TISoft. It is small enough to upload. Regards, billwest Update, Softshop has returned to the CA01 Catalog and can be purchased from Siemens. |
Last edited by: billwest at: 5/29/2012 3:21 PM |
|
12/10/2009 4:43 AM | |
Posts: 26 Rating: (1) |
Hi billwest, I have same expectation with Mr. danga Thank U. |
12/16/2009 6:08 PM | |
Posts: 510 Rating: (117)
|
TISOFT is no longer in the CA01 catalogue so I have attached it. The manual is still available for download. I recommend you download it if you are not familiar with TISOFT installation.
AttachmentTISOFT.zip (8272 Downloads) |
This contribution was helpful to14 thankful Users |
12/23/2009 3:33 AM | |
Posts: 26 Rating: (1) |
billwest.... Arigato, Thank You, Mercy, Terimakasih... |
3/17/2015 3:58 PM | |
Posts: 1 Rating: (0) |
Hey Billwest: Is 7.1 backwards compatible with 6.31? We currently have 6.31 at our site. Do you have a copy of that? Thanks, |
2/11/2019 10:29 AM | |
Posts: 3 Rating: (0) |
Hello 1. Is TISOFT it free Software and anybody can use this ? 2. If not How to get Software officially ? Regards kantha
|
Follow us on