4/5/2024 9:18 AM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Please also see the attached screenshots. We have had a WinCC client added to some of our machines to increase the flexibility for the operators. But when I open the WinCC client there are no process pictures and only internal tags. I'm thinking that all the maintenance and modifications in the WinCC project must be done in the WinCC server and then they will automatically be mirrored to the clients. Is this correct and when can I see this in my project(s)? In general - how do I keep the client (process pictures, warnings, alarms and events) synchronized when I have one (or more) client(s)? AttachmentServer_client.zip (12 Downloads) |
4/17/2024 11:14 AM | |
Joined: 8/3/2009 Last visit: 5/15/2024 Posts: 12951 Rating: (1650)
|
Hello xmnj you can also use a WinCC Client without an own project. for this you will not have to set the WinCC Application in Simatic Manager. Just insert in Computerlist in Server project and do a interconnect with Simatic Shell or WinCC autostart on the WinCC Client. https://support.industry.siemens.com/cs/de/en/view/109771695 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on