3/21/2024 2:42 PM | |
Joined: 10/3/2022 Last visit: 6/2/2024 Posts: 51 Rating: (0) |
Hi Riddersholm As for the PLC program, the subroutine being used for the Handwheel is exactly the same as the one in Tool Box examples. Attached you can find the whole OB program and the subroutines linked to the handwheel. I am also attaching the example from the Tool Box from where i got the handwheel subroutine. As for the .ard file I still did not do that, as I am not in the workshop for the next 2 days. Can you in the meantime check the PLC program please? Is there something wrong or that I need to activate somewhere else? AttachmentHandwheel.zip (48 Downloads) |
Follow us on