12/19/2022 5:12 PM | |
Joined: 2/10/2020 Last visit: 2/16/2024 Posts: 6 Rating: (0) |
I have tried to reset, Format memory card. Nothing worked. |
12/29/2022 2:15 PM | |
Joined: 8/6/2018 Last visit: 6/4/2024 Posts: 251 Rating: (39) |
Hello, Have you tried to put the PLC card in the PC and load directly on the card? Thanks you |
12/30/2022 7:27 AM | |
Joined: 3/11/2019 Last visit: 6/4/2024 Posts: 1453 Rating: (263) |
Hi, trying to download directly to the SMC is a good recommendation. If you will do this with TIA directly, you may run into the same message. But you can try Option "3" from following FAQ: How do you create the project data for the SMC so that you can download the project to the S7-1200/S7-1500 CPU even without STEP 7 (TIA Portal)?After you generated the file "S7_JOB.SYS" and the folder "SIMATIC.S7S" in an folder on the PC, you can manually copy/paste the file "S7_JOB.SYS" and the folder "SIMATIC.S7S" to the SIMATIC Memory Card with the Windows explorer. Important: Do not format the SMC with windows! regards sancruz |
Feedback appreciated, please rate |
|
Follow us on