5/30/2012 1:54 PM | |
Posts: 1530 Rating: (59)
|
Hallo Dony_C, could it be possible that you have got a "Connectivity Pack License" on your computer which is working without any problems? Part of Manual: Access to WinCC User Archives using Microsoft OLE DB requires a Connectivity Pack license on the computer where the WinCC user archives will be accessed. Best regards Bizur |
5/30/2012 2:10 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
your IPC427C is running Windows Embedded Standard 2009? It seems like it's missing a registered version of the Microsoft Datagrid Control |
B r g d s , |
|
6/6/2012 7:52 AM | |
Posts: 291 Rating: (68) |
Hi Dony, Please find the attachment and execute the two .reg files step by step. Then reboot your IPC, you'll find the "Microsoft DataGrid Control, Version 6.0" available in WinCC Graphics. Good luck, Komi P.S. Microsoft DataGrid Control 6.0 (SP6) (OLEDB) owns a CLSID: {cde57a43-8b86-11d0-b3c6-00a0c90aea82} In case the reg files can not solve your problem, try check the CLSID of your "Microsoft DataGrid Control, Version 6.0 (OLEDB)" and modify what in the Step2_xxx.reg (Mine is "SP6".) Anyway, it works!! AttachmentNeeded_Reg.zip (242 Downloads) |
4/21/2024 12:42 PM | |
Joined: 7/15/2022 Last visit: 5/16/2024 Posts: 7 Rating: (0) |
I have the same problem but this procedure did not help me. Can u any idea? |
4/25/2024 9:52 AM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1650)
|
Hello there is also a Option from Siemens for a grid control: PM-Grid Control https://support.industry.siemens.com/cs/de/en/view/109806438 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on