1/14/2017 4:09 PM | |
Joined: 7/3/2016 Last visit: 5/17/2024 Posts: 24 Rating: (0) |
Hello, I have a Siwarex U module (7MH4950-1AA01) and it happened when I send, via faceplate, the commands to configurate zero/weighted calibration, the faceplate get freeze, send/recibe bottoms comes grey and never comes back to normal state, the only solution is power off the ET200M (6ES7 153-2BA02-0XB0), in other hand I used de APL interface (Block SiwaU08), when send the calibration I saw two outputs interesting, the GrpErr (Group error) its always high, but when get visible almost all the outputs that the module help considerate part of the "group", they dont show any specific error, other output that comes high and remains in that state is CmdInpr (Command in progress) in the same time when I push botton send throught the faceplate. Locally I used siwatool and get a full calibration of module without any troubles. I don't find any refrence to similar case in the forum, Please, you could send me any suggestion. Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/16/2017 1:28:42 PMNew subject after splitting |
|
2/1/2017 2:59 AM | |
Joined: 7/3/2016 Last visit: 5/17/2024 Posts: 24 Rating: (0) |
|
2/1/2017 7:33 PM | |
Joined: 7/3/2016 Last visit: 5/17/2024 Posts: 24 Rating: (0) |
|
2/1/2017 7:33 PM | |
Joined: 7/3/2016 Last visit: 5/17/2024 Posts: 24 Rating: (0) |
|
Follow us on