2/28/2024 10:54 PM | |
Joined: 1/29/2020 Last visit: 4/4/2024 Posts: 5 Rating: (0) |
j'ai un problème pour communiqué le PG avec SIMODRIVE 611 (l'entrainement 6SN1123-1AB00-0CA3) (carte régulation 6SN1118-ODM33-0AA0) via câble adaptateur USB-SIMODRIVE 611 pour récupérer les paramètre de variateur défectueux pour le replacer pou un nouveau variateur ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/29/2024 11:49:52New subject after splitting |
|
2/29/2024 11:50 AM | |
Joined: 8/21/2014 Last visit: 5/24/2024 Posts: 959 Rating: (13) |
Hello R.ouba Please try to discuss your question in English language. This is an internationalcommunityand we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
Best Regards, The Helping Hand |
My Forum is the place to personalize your profile, |
|
3/1/2024 3:10 AM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
Hi, R ouba, let me answer your question: 1st of all PG is a PC, any communication need software, you did not say what is your SW? 2nd SIMODRIVE 611 Family had 3 kinds of control --611A,611D, and 611U so your control board 6SN1118-0DM33-0AA0 IS NO POSSIBLE COMMUNICATION WITH PG. 6SN1118-ODM33-0AA0 is 611D control, it is only communicate with 840D NCU Hope you can post picture to show what is SW. and show picture of your control card, may be you post a wrong number? ============================================================= I have a problem communicating the PG with SIMODRIVE 611 (drive 6SN1123-1AB00-0CA3) (control board 6SN1118-ODM33-0AA0) via USB-SIMODRIVE 611 adapter cable to recover the parameters of the faulty drive and replace it with a new drive.
|
Last edited by: nulizhang at: 03/02/2024 02:46:17If you like my comments please |
|
3/15/2024 10:43 PM | |
Joined: 1/29/2020 Last visit: 4/4/2024 Posts: 5 Rating: (0) |
HMI PICTURE |
3/17/2024 2:13 AM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
I told you 611D cannot use SIMO COM U. if you want to understand 840D and 611D, you need download "SINUMERIK 840D, 611D Start Up Manual" to read carefully. See my attached picture: what I draw red line, between NCU and 611D there is drive bus transfer drive data, from NUC to PCU50 there is MPI cable --continue transfer drive data to PCU50, you can read drive data, or change (password protected), you can back up drive data to PCU50 save data into HDD. so from beginning you did not have good idea. so your question should be No question if you can understand my this writing
Attachment840D_611D_HMI.pdf (50 Downloads) |
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
Follow us on