6/18/2009 3:03 PM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi please check the link for simodrive manual http://support.automation.siemens.com/WW/llisapi.dll?query=docon+web&func=cslib.cssearch&content=skm%2Fmain.asp&lang=en&siteid=csius&objaction=cssearch&searchinprim=0&nodeid0=10805517 find attached gsd files regards ram Attachment611u.zip (200 Downloads) |
This contribution was helpful to1 thankful Users |
6/18/2009 3:41 PM | |
Posts: 271 Rating: (29) |
Hello Wincc, As compared to the MM440 the Simodrive 611U is a multi-axis drive. It is possible to operate standard induction motors with output frequencies up to 1500 Hz, 1FT6/7, 1FK6/7, 1FE1, 1FW3, 1FW6 and1FN1/3, etc. The drive can be operated in both velocity and basic positioning modes. It also can be operated in torque/current mode. U stands for Universal which essentially means it can power practically all types of motors and it can operate in multiple modes. There are 256 traversing blocks that can be programmed. I encourage you to get a copy of SimoCom U software for commissioning and diagnosing. It can be downloaded from http://support.automation.siemens.com/WW/view/en/10804940/133100. This is a generic Simodrive download site and you may want to download the latest version (i.e., V12.1). Documentation is available at http://www.automation.siemens.com/doconweb. Hope this helps... |
6/19/2009 2:50 PM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear All Thank you for your posting. I think it may helpfull to me. |
3/17/2024 6:29 PM |
|
Joined: 12/22/2010 Last visit: 5/25/2024 Posts: 97 Rating: (0) |
Simodrive |
Follow us on