12/28/2005 4:27 PM | |
Posts: 52 Rating: (8) |
Hi,all Can anybody tell me which CPs can communicatevia modbus-tcp/ip? Thanks. hannibar |
1/9/2006 3:11 PM | |
Joined: 4/3/2007 Last visit: 4/15/2024 Posts: 35 Rating: (5) |
Hello CP 441 can communicate via modbus. Take a look under http://support.automation.siemens.com/WW/view/de/4332922 CP 341 can communicate via modbus. Take a look under http://support.automation.siemens.com/WW/view/de/4337574 kind regards |
1/18/2006 1:52 PM | |
Posts: 52 Rating: (8) |
Hi,Late Would you please tell me how can I get these FUNCTION BLOCKs! King regards, hannibar |
1/18/2006 2:09 PM | |
Joined: 8/25/2005 Last visit: 6/5/2024 Posts: 1162 Rating: (110) |
Hello hannibar, I'm not sure wether this is the right information or not: [:(] In the documentation Loadable Driver for Point-to-Point CPs MODBUS Protocol RTU-Format S7 is Master I found the information, that the datatransfer between CPU and CP in the S7-400 are the SFBs BSEND and BRCV (capture 6.2) This SFBs you will find in the Standard Libary within STEP7. Best regards Sabine |
1/19/2006 5:55 AM | |
Posts: 52 Rating: (8) |
Hulzhex, This is only about modbus but not modbus-TCP/IP! regards hannibar |
1/22/2006 7:04 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316) |
Hello Hannibar, Please send a email address to me then i can send you the handbook. [:o] Best regards, Late I make in a few days a attachement so that you have the handbook and the address to buy the FB, i don't have the information on this computer. [:blush:] Attachment18528717 Open Modbus - TCP e.pdf (1132 Downloads) |
Last edited by: Late at: 1/26/2006 6:31 PMpdf toegevoegd Last edited by: Late at: 1/22/2006 7:40 PMLast edited by: Late at: 1/22/2006 7:37 PMI hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/27/2006 6:37 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316) |
Hi Hannibar, AttachmentOpen Modbus TCP.pdf (1027 Downloads) |
Last edited by: Late at: 1/27/2006 8:07 PMAttachement with the ordering information and some discription. I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
2/6/2006 4:53 AM | |
Posts: 52 Rating: (8) |
Late, Thank you very much! King regards! hannibar |
Follow us on