12/24/2022 7:52 PM | |
Joined: 6/1/2020 Last visit: 5/13/2024 Posts: 37 Rating: (0) |
I have a project in WinCC Flexible 2008 in which I have a MP370 panel. I the settings of the device, I have checked act as OPC server, that is the unique parameter that I have to check according to the documentation, if I am not wrong. Then I run the project in the simulator, and with an OPC DA client, in this case I am using the integration objects data access explorer, that is a free application [snip] I see this servers: But I don't know which is the correct server where I have to connect, I don't set the name of the server in the WinCC project. I only can connect to one, but there is not tags in this server, so it is not the correct one. I have run a example project of siemens, but the server names is the same than if I run my project, so I am thinking that the server is configurated apart of the application. How could I see the tags that I have in my MP370 panel? EDIT: I am following this documentation: https://support.industry.siemens.com/cs/ca/en/view/22701694 And in OPC XML Manager y set the prefix and the IP. If I set the prefix for example as MP370B, in the OPC XML client, in this case Integration Objects OPC Data Access, I can open the tags browser and I see this: So it can find the server, MP370B, but I can't see any tag. |
Last edited by: Jen_Moderator at: 12/26/2022 10:09:56Link removed, as it's an advertisment. Last edited by: GTSAGarcia at: 12/26/2022 12:32:15 |
|
12/29/2022 7:36 AM | |
Joined: 6/19/2017 Last visit: 6/3/2024 Posts: 8103 Rating: (165) |
Closed cause question posted twice. The second thread with the subject How to configura the OPC server in a MP370 panel? is published within the conference SIMATIC WinCC flexible. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on