12/16/2021 2:32 PM | |
Joined: 4/22/2020 Last visit: 1/10/2024 Posts: 2 Rating: (0) |
Hello I am attempting to create the Send Email example JScript Edge app, using the steps outlined here: Creating and managing Edge apps using the example of the ""SendMail"" app (siemens.com) When I run the scripts on my host Windows PC, they run fine, connecting to the Unified runtime. However, when I build the app in Docker and attempt to run it, I get the following error:
The issue seems to stem from running the code in Linux, particularly the "get_pipe_name" function from the opn.js file. I can also see the issue was raised previously, but there was no resolution identified there: Has anyone had success in building an app that communicates using OpenPipe and running it using docker or in Linux? Any help would be greatly appreciated. Thanks. Attachment109778780_SendMail_EdgeApp_V11_en.pdf (636 Downloads) |
Last edited by: Jen_Moderator at: 12/17/2021 09:44:00Added PDF from link as an attachment. |
|
Follow us on