2/28/2010 6:00 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Dear Shaun, It is only a possibility to get a good connection to the MPI or PROIBUS. It is depending if this 24V is coming to the Sub-D connectorif the connected device have on the right pin 24V. Which display are you using ? Look in the networkbookSIMATIC NET PROFIBUS Networks for further information on which pin the 24V is normally. Chapter 4.7 and further give more information about the busterminal. On page 5-4 the layout of the connector is showed (Pin 2 Massa 24V and Pin 7 +24V). You can make a Sub-D connector which is connecting to the Pins 3 and 8 and which is only have on Pin 2 and 7 a external 24V power supply. Take care that the 24V is fused and that it won't come on the other Pins, you may damage the equipment... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to1 thankful Users |
3/1/2010 8:06 AM | |
Joined: 10/7/2005 Last visit: 5/6/2024 Posts: 3004 Rating: (1046)
|
Hello shaun can you please check if you have the power LED on the your MPI Adaptor lit? As Latealready said, the "normal" USB MPI/DP PC adaptorneeds 24V from theMPI/DP port to which it is connected (Pin7: +24V, Pin 20V. I can't remember if the older RS232 version needed it too). The busterminal does however NOT provide these 24V to Pin 7&2 whichmay very well be your problem. If you have a Field PG, CP5511 or 12 PCMCIA cardshandy you could also test it first with these (they do NOT need the 24V supply from Pin 7&2). Btw, you can also order a seperate 24V external power supply adaptor for the USB MPI/DP Adaptor(part number and link 6ES7972-0CA00-0XA0)
Providing you get 24V power to your MPI Adaptor I think it will work (MPI is a subset of Profibus and I don't think that thebusterminal will "block" it. I have however never tested this one). I hope this helps |
Cheers |
|
Follow us on