1/7/2022 1:45 PM | |
Joined: 10/1/2015 Last visit: 4/26/2024 Posts: 17 Rating: (0) |
Hi, i have same problem. 2 F-PLC (1515TF and 1517F) connected with profinet. I have 2 projects so i used pdf, chapter 2.2 (Configuring IO controller and I-device cross-project) https://support.industry.siemens.com/cs/document/109478798/configuration-and-application-of-the-profinet-i-device-function?dti=0&lc=en-WW Ichecked HW identifer, put timeout to 500ms, check DP_DP_ID that match corectlly... Sending data from PLC (defined as IO-device) to PLC (defined as IO-Master) everything is working super. Sending data from PLC (defined as IO-Master) to PLC (defined as IO-device) there is an error. Error happens when i trigger signal on true which i am trying to send. On SENDDP (PLC IO-master) i get status error 16#10 (byte) on RECVDP(PLC IO-device) i get status error 16#40. I checked help, but cant find solution.I am using TIA 17 on both projects. Thank you for your help ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 01/09/2022 22:18:58New subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/14/2024 12:42 AM | |
Joined: 4/14/2024 Last visit: 4/14/2024 Posts: 1 Rating: (0) |
我有同样的问题,请问最后是怎样解决该问题的,SendDP 为16#10,RCVDP为16#40. |
Follow us on