Industry Online Support
Technical Forum
8/2/2010 8:14 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User boopathi@sequent wrote: Dear All, In wincc 7.0 i have to use check box for the following application. 12 number rtd value available in tag but customer has to select few number only that value we have to sum and send to pid pv input.send the sample code and use of checkbox or any oter way configure. |
8/2/2010 3:30 PM | |
Posts: 79 Rating: (0) |
Hi, please send me the checkbox c script .sample |
8/4/2010 2:34 PM | |
Posts: 79 Rating: (0) |
Dear Romulus, i attached what i need exactly.i have to do with checkbox 12 number of selection box i configured and will select 4 means in tag i have to get 4 value. i selected 8 means hmi runtime tag will get 8 value.like that howmany number will select according to will get value. for above mentioned application how to write script explain me .send the script AttachmentNewPdl0.pdf (884 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on