3/19/2024 6:47 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452)
|
Hi, Since the CPU has no on-board peripherals, an additional module is required. When configuring the device with the TIA Selection Tool, the following modules are offered for counting:
Of course, you have to decide which one fits your needs. However, I would suggest that you contact the Siemens Technical Consulting in your region. Kind regards |
This contribution was helpful to1 thankful Users |
3/19/2024 7:15 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452)
|
Hi, As you can see from the specifications of ET 200SP, TM Posinput 1 (6ES7138-6BA01-0BA0), this module supports both 5V TTL and RS-422 (SSI). Kind regards |
This contribution was helpful to2 thankful Users |
Follow us on