5/7/2024 2:16 PM | |
Joined: 8/12/2021 Last visit: 6/4/2024 Posts: 309 Rating: (29) |
Hi! In that case, it is very possible that the card is damaged. As far as I understand, the LEDs should indicate some status. Try to verify the power of the module. |
If this Information really helps, you could use the Rate function |
|
5/8/2024 8:00 AM | |
Joined: 3/11/2019 Last visit: 6/4/2024 Posts: 1453 Rating: (263) |
Hi, does the cpu itself show an error? Is there an entry in diagnostics buffer of the CPU? You can also upload the diagnostics buffer as .txt file. Is the singal board recognized in the online diagnostics and if yes, are there any entries in the module diagnostics of the board directly? Meaning of status LED can be found here: Status LEDs-> Status LEDs on a signal board (SB) SB 1221 200 kHz digital input specifications-> Table: Wiring diagrams regards sancruz |
Last edited by: sancruz at: 05/08/2024 08:04:15Feedback appreciated, please rate |
|
Follow us on