12/4/2008 12:51 PM | ||||||||||||||||||||
Posts: 510 Rating: (117)
|
Does this help? Configuring protocol parameters Parameters to be setTo edit the parameters, double-click "Communication > Connections" in the project window of the HMI device. "SIMATIC 500/505 DP" is selected in the "Communication drivers" column in the work area. Change the protocol parameters of the connection in the Properties window. Device-dependent parameters
PLC-dependent parameters
The settings in WinCCflexible must match the configuration data of the interface module, for example CP5434 DP.
billwest AttachmentTI505_Profibus_WinCCFlex .pdf (690 Downloads) |
|||||||||||||||||||
Last edited by: billwest at: 12/6/2008 3:41 PMI have added a document that may assist as well |
||||||||||||||||||||
Follow us on