5/11/2024 4:43 PM | |
Joined: 12/22/2012 Last visit: 6/4/2024 Posts: 91 Rating: (4) |
I faced with the same bottle neck of UDT. I defined a struck tag which contains 16 boolean tags at the input of a FB. I wanted to pass the image of an input word and to the struck bits. I could not write source word address to the input of FB. It is same for the outputs. I defined a word/int output at the FB. I can not copy the content of a struck tag(contains 16 bits) to this output as a word. I do not know whether is it a bottle neck or a bug at TiaPortal v17. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2024 09:23:42New subject after splitting |
|
5/13/2024 9:24 AM | |
Joined: 6/19/2017 Last visit: 6/7/2024 Posts: 8150 Rating: (165) |
Closed cause question posted twice. The second thread with the subject how to copy 6 word image on tags defined as struck type at static part of a DB is published within the conference STEP 7 (TIA Portal). Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on