13.05.2016 07:42 | |
Beigetreten: 11.10.2006 Letzter Bes: 30.05.2024 Beiträge: 5854 Bewertung: (793)
|
Hello vonfluez, please have a look at the function diagram 10 in the attached documentation, the receive words in the CUVC depend on the T100 parameter settings, as the Com Board values are received from T100 and the receive data in CUVC are the values from T100. DateianhangMS100_e.pdf (384 Downloads) |
With best regards, |
|
13.05.2016 08:31 | |
Beigetreten: 15.12.2006 Letzter Bes: 23.04.2024 Beiträge: 50 Bewertung: (4) |
Thank you for the documentation! Now I can better analysis what's happening. This will take awhile. |
Folgen Sie uns auf