7/3/2023 4:17 AM | |
Joined: 1/17/2019 Last visit: 7/4/2023 Posts: 1 Rating: (0) |
Hi! What steps should I take to replace CPU 6ES7315-2AF03-0AB0? Which CPU is recommended for replacement? What possible problems? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/03/2023 12:04:30New subject after splitting |
|
7/3/2023 12:29 PM | |
Joined: 5/6/2022 Last visit: 5/23/2024 Posts: 420 Rating: (83) |
Hi AndreVZ, From what I have been able to find, the successor of the 6ES7315-2AF03-0AB0 equipment is the following: 6ES7315-2AF03-0AB0 -> equivalent to 6ES7315-2AH14-0AB0 controller requires MMC card, eg 6ES7953-8LJ31-0AA0 You can find more information in the discontinuation note that I share below: "Discontinuation of the S7-300 CPUs of the first generation and associated memory cards" You will also find information to keep in mind when making the change of equipment. You will have to modify the project by changing references. I hope it can help you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
7/4/2023 8:26 AM | |
Joined: 3/13/2009 Last visit: 6/4/2024 Posts: 131 Rating: (1) |
If you replace the cpu with an identical one you just need to remove the cpu,install the new CPU and then place the memory card of the old cpu in the mmc slot of the new cpu and then power up and run the cpu. But if the new plc is not identical with the old one then first of all you should have access to the S7 project or upload it from the old cpu then you should replace the old controller with the new one in the hardware configuration (simatic manager) and finally upload the project to the cpu. for the type of cpu you should select a type that its functionality and performance is higher to be on the safe side. but in many applications the selected cpu is much higher than required . |
This contribution was helpful to1 thankful Users |
Follow us on