4/18/2024 4:12 AM | |
Joined: 1/14/2020 Last visit: 4/23/2024 Posts: 3 Rating: (0) |
Dear Experts, I have a scenario that using S7-1200 as Modbus Master to check number of Modbus Slaves and which of it is alive, so that the Master knows what to do/message with other Slaves.
During an online search, found the Library for Modbus RTU (LMRTU) https://support.industry.siemens.com/cs/us/en/view/109747565 In the documentation, it only mentioned CM1241, and this library still in the era of TIA V14, I think that should be still valid. Is that also possible to use Library for Modbus RTU (LMRTU) with CB1241? I am using TIA V17. Currently I don't have multiple CPU to test with because this is before the purchase, now deciding to whether use CB1241 or CM1241. Thanks!! nicki |
Last edited by: Jen_Moderator at: 04/18/2024 10:21:51Link optimized. |
|
4/18/2024 6:19 AM | |
Joined: 1/14/2020 Last visit: 4/23/2024 Posts: 3 Rating: (0) |
Thanks for you great help! |
This contribution was helpful to1 thankful Users |
Follow us on