11/8/2023 2:32 AM | |
Joined: 8/6/2023 Last visit: 11/28/2023 Posts: 5 Rating:
|
Hi everybody I need some help , because I have a problem with a Simotion D445. The problem is that appear this alarm, and stop all the servos, and we have connected the encoder to a adapter to PILZ PNOZ m1p, and then to a SMC 20 (Siemens) and go to the simotion. Technological alarm TO_Axis_08: Alarm Error 20005 : Device type:1, log. address:660 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_07: Alarm Error 20005 : Device type:1, log. address:620 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_06: Alarm Error 20005 : Device type:1, log. address:520 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_05: Alarm Error 20005 : Device type:1, log. address:480 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_02: Alarm Error 20005 : Device type:1, log. address:360 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_01: Alarm Error 20005 : Device type:1, log. address:320 faulted. (Bit:0, encoder number:0, reason: 0x4h) TO_Axis_03: Alarm Error 20005 : Device type:1, log. address:400 faulted. (Bit:0, encoder number:0, reason: 0x4h) This is file Diagnostics Buffer when an error occurs I don't find which it's the problem that occur this alarm, I hope you can help me with this problem. Thanks and I appreciate your support.
AttachmentDevice Diagnostics - [D445]_error.txt (339 Downloads) |
11/10/2023 8:51 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating:
|
you must check when the error is present, or check fault history in the drive |
11/10/2023 9:06 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating:
|
the diagnostic log is not the complete log, so why i should check it? |
11/10/2023 9:13 AM | |
Joined: 8/6/2023 Last visit: 11/28/2023 Posts: 5 Rating:
|
Sorry, did you want this file?
AttachmentDevice Diagnostics.txt (283 Downloads) |
11/10/2023 9:23 AM | |
Joined: 8/6/2023 Last visit: 11/28/2023 Posts: 5 Rating:
|
Can you explain in more delail? please... |
Follow us on