5/24/2018 8:40 AM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Please see attached screenshots (when will Siemens make it possible to attach more than one pic without packing them into a single file?) I need to download some minor modifications to a machine. One of the modifications is in a "standard" FC block so I assume I can just download that one and it will automatically be compiled and all is well. The other modification is in a safety FC block and that might be different. What is the right way to download the safety FC - should it be compiled somehow first ? Do I need the Safety password to download the safety block (as I would to edit it)? AttachmentUR Modifications.zip (277 Downloads) |
Last edited by: xmnj at: 5/24/2018 9:33:07 AM |
|
5/25/2018 1:24 PM | |
Joined: 10/16/2007 Last visit: 2/23/2024 Posts: 627 Rating: (45) |
If you have installed the safety option and you open "your" safety block you need the Password. In the SIMATIC Manager under Extras you find the item edit safety program. I attach a creen shot what it looks like. It is in German but within this tool you translate the safety blocks and transfer them to the CPU. Also you activate the safety function inside the CPU and so on. Regards AttachmentSafety.pdf (453 Downloads) |
Follow us on