4/16/2024 6:18 AM | |
Joined: 10/3/2023 Last visit: 5/7/2024 Posts: 27 Rating: (0) |
Hello Everyone, I have an old panel PC670 (6AV7724-1AC10-0AD0) and it has winCC explorer. It has the format of (.mcp) and i have an my old customer project to download in the Panel PC670. this project is protool project. it is (.pdb) format. How to download my protool project into the panel pc670? how to convert my protool project(.pdb) into wincc project (.mcp) ? Also, I don't know the procedure to download into the pc670? Uploaded my project for ur Reference. ------------------------------------------------------------------------------------------ AttachmentPC670.zip (23 Downloads) |
Last edited by: Riyasa at: 04/16/2024 06:19:45Last edited by: Jen_Moderator at: 04/16/2024 11:00:55New subject after splitting |
|
4/16/2024 2:51 PM | |
Joined: 7/19/2022 Last visit: 5/21/2024 Posts: 358 Rating: (61) |
Hello Riyasa, The .mcp file corresponds to a WinCC V7.x project while .pdb file corresponds to an application made by Protool. They are different environments and concepts. A Protool file cannot be migrated to a WinCC SCADA application. On the PC you should have the Protool Runtime installed and load the PDB as indicated in the manual (from page 55): SIMATIC HMI ProTool/Pro Runtime |
If this Information really helps, you could use the Rate function |
|
4/22/2024 11:37 AM | |
Joined: 10/3/2023 Last visit: 5/7/2024 Posts: 27 Rating: (0) |
Hi JBS98 I installed Protool Runtime in my panel PC670 and now it's working. but I don't have a protool license and it is showing demo version. my question is ' Is demo version will work as the licensed version? |
Follow us on