5/16/2024 11:29 AM | |
Joined: 5/16/2024 Last visit: 5/16/2024 Posts: 1 Rating: (0) |
Hi everyone does anyone know how to add more message rows to the PCS7 message system, there are 22 at the moment and I want to add more, i have a attached a screen shot of the dialog box. Thanks Heath ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 05/16/2024 13:44:51New subject after splitting |
|
5/16/2024 6:56 PM | |
Joined: 2/1/2010 Last visit: 5/29/2024 Posts: 144 Rating: (70) |
You can manually make extra message classes in WinCC, but I believe there is no way to get them back into the PCS7 message system interface. I don't really recommend making manual message classes because of this, they are only available for manually created WinCC alarms, not ones created through compilation. Based on your screenshot you might be able to further optimize the 6 configurable message classes to make 6 unique classes to give you the features you need instead of H/L class for each alarm, warning,tol. That is the best practice route. |
If my post helped you, please rate. Thanks. |
|
Follow us on