9/18/2023 5:11 AM | |
Joined: 9/18/2023 Last visit: 9/18/2023 Posts: 1 Rating: (0) |
I can not setup STARTER 5.5 HF1, The fault is: The installation files integrity check was not succesful! Details see log file CheckIntegrit.log Setup will be aborted without installation! Note: With silent installations, the SetupMode.ini file must be copies into another directory and change. The Setup.exe must then be called with the <path>\SetupMode.ini parameter. PLEASE HELP ME! THANKS
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/18/2023 11:48:19New subject after splitting |
|
9/18/2023 8:41 AM | |
Joined: 5/12/2006 Last visit: 6/12/2024 Posts: 22262 Rating: (2989)
|
have you check the logfile? Have you check the sha crc that this is correct for the downloaded files? |
10/20/2023 2:55 AM | |
Joined: 6/10/2020 Last visit: 4/15/2024 Posts: 1 Rating: (0) |
Very helpful, thanks~ |
Follow us on