3/25/2007 9:26 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580) |
Hi dmg, it is possible to convert the output of a counter block into values. Look at the example in the small LOGO-Programm. The number of pulses must be translated into a multiplexer and then you use one or more analoge amplifier to convert the value of the conterin a value of phys. units. To set the number of decimalsto n (1 to 5) it is equal to dividide by 1/n. But remember that the maximum value is not so big as the counter can count !!!Do notforget to clear/reset the counter by the USER.If you wont additional to convert impulses per time to a phys. unit look my comments at the german forum under: 1) velocity in thediplay 2) strokes per minutes
AttachmentPulses_to_Units.zip (870 Downloads) |
==> Meine TAG-Listen: "deut." |
|
3/25/2007 9:49 PM | |
Posts: 12 Rating: (0) |
Dear Betel, Many thanks for the elegant solution! Best regards, Dimitri |
Follow us on