4/25/2024 7:46 AM | |
Joined: 1/2/2024 Last visit: 5/14/2024 Posts: 20 Rating: (0) |
In the subject of "Memories" i have something that i don't understand ? P.S : check the "memory to output" picture to understand meeeeeeee. 1- Version 2 is something i stumbled upon in the program installed in the s7-400 in my line of production and it's used extensively throughout the program. My question is, what are the benefits and utilities of storing data in a "memory" then sending to the "output" instead of sending to the "output" directly ? (Version 1 is what i usually use). 2- If Version 2 is more beneficial and professional should i do something like this for a "water level detector" for example : 2.1- create a memory e.g "m_water level" type "int" (use a "SCALE" to translate the value). 2.2- create an input called "water level". 2.3- use a "MOVE" to transfer "m_water level" to "water level" Posted by N00b_Lvl_ONE_THOUSAND ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_5311751 at: 04/25/2024 07:46:45Last edited by: Jen_Moderator at: 04/25/2024 09:17:31New subject after splitting To reach level ONE THOUSAND... It's hard work !!! |
|
Follow us on