Search result

246 machines were found

Specifically, at this edition of the EMO Danobat is to present a fully automated system for grinding the injector seal on automotive engines, a component barely 2 mm in diameter for which production ...
  • Hall: 11
  • DANOBAT S.Coop.
Specifically, at this edition of the EMO Danobat is to present a fully automated system for grinding the injector seal on automotive engines, a component barely 2 mm in diameter for which production ...
  • Hall: 11
  • DANOBAT S.Coop.
The Omicron CNC grinding machines now benefits control enhances ease-of-use with a customised graphic interface and grinding cycles with simple and intuitive software further aiding the grinding proc...
  • Hall: 11
  • ROBBI Group S.r.l.
Dynamic and productive machining in five axes. With HF 3500. Fifth axis provided by the workpiece for dynamic 5-sided machining and simultaneous 5-axis machining NC-Rotary indexing table with ...
  • Hall: 12
  • Gebr. Heller Maschinenfabrik GmbH
High precision, multitasking machining center for 5-axis simultaneous machining as real gantry type. Travel dist.: X, Y, Z = 1,000, 1,200, 800 mm Working area diameter: 1,220 mm A-axis +- ...
  • Hall: 12
  • ALZMETALL GmbH & Co. KG
MultiTec is WALDRICH COBURG´s smallest machining centre with a modular design. It can of course be adapted in various ways to suit all special requirements of our customers. For example, the length, ...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
FLA means maximum productivity and flexibility into a series of high-speed, movable bridge 5-axis CNC machining centers able to answer the manufacturing needs of any specific application field . Amo...
  • Hall: 13
  • BELOTTI S.p.a
Wthin the range, the TANK.G family represents an evolution of the TANK model. Of it, it maintains the same attention to the production process, a guarantee of excellent precision, and is distinguishe...
  • Hall: 13
  • MCM SpA
POWERTURN 2000 C1 Multifunctional vertical CNC mill-turn Robust frame of the machine Powerful drive of rotary table Rotary tool drive and conrolled C axis positioning for milling, dril...
  • Hall: 13
  • TOSHULIN, a.s.
UNIKA is a high speed-milling machine with movable column. The movements of the main axes are obtained by means of linear motors (chilled by water) (gantry on vertical axis) and allows a rapid feed o...
  • Hall: 13
  • O.M.V. Officine Meccaniche Venete S.p.A.
Perfect for a wide variety of workpieces! TAURUS is the ideal machining center for the following applications ... Steel construction; frames, railway bogies, fixtures, housings Gearbo...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
Complex 5-axis processing machine with integrated tool magazine.
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
The strength of the machines of the VT-series lies in their 4-axis machining of large quantities of shafts of up to 630mm in length. Since the machine concept comprises a fully integrated autom...
  • Hall: 17
  • EMAG GmbH & Co. KG
The successful model is now also available with the Sinumerik 840D sl controller from Siemens, which makes the WF 410/610 MC even more flexible. In addition to manual handwheels, the hybrid machine f...
  • Hall: 17
  • Kunzmann Maschinenbau GmbH
EMAG LC 4-2: The new autonomous laser cleaning machine With the LC 4-2, a standardized, modular system for laser cleaning has been designed for components with a maximum diameter of 200 mm and a...
  • Hall: 17
  • EMAG GmbH & Co. KG
Falling batch sizes due to the individualization of products and just-in-time production pose new challenges to industrial manufacturing in competition. With the new ECX series Schütte offers the sol...
  • Hall: 17
  • Alfred H. Schütte GmbH & Co. KG
The integrated combination of diverse technologies and methods is one of the definitive trends in modern manufacturing. Apart from the generous standard equipment, such as turning-milling spindle and ...
  • Hall: 2
  • DMG MORI
The CTX beta 4A series offers a compact high-performance turning center for the demanding 4-axis complete machining of bar, shaft and chuck parts. The working area concept with two VDI 40 star turret...
  • Hall: 2
  • DMG MORI
Flexible gantry loading system for maximum productivity Low height of 3.4 m by means of telescopic axle Workpiece weight up to 2 x 15 kg with double gripper Small footprint of 10.2 m Control...
  • Hall: 2
  • DMG MORI
MX9 MX9 is a high performance 5 axis machining center with high machine dynamics. The FEM-optimized MX-multifunctional series design accommodates high clamping devices or machining of work piece...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Famar Srl 2 Hüller-Hille 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Priminer machine tools Dongguan Co.,ltd 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Shandong DEED Precision Machine Tool Co.,Ltd 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 Samputensili Machine Tools 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 XYZ Machine Tools Ltd 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter